Technical FAQs

Ask a Question

How many high speed counters and pulse train outputs are available in Magelis XBTGC2230T/U.

Magelis XBT GC 2230T/Uhaving 16 Inputs 24VDC and16 Transistor Outputs 0.5A capabilities have 4 High Speed
Counters(Maximum Frequency 100KHertz)a
nd 4 Pulse Train Outputs(Maximum Frequency 65 KHertz).
Was this helpful?
What can we do to improve the information ?