Technical FAQs

Ask a Question

What is significance of communication module SR3NET01BD.

Zelio Logic modular smart relays are connected to the Ethernet network via the Ethernet server communication module.
Communication module SR3NET01BD allows communication on the Ethernet network under the Modbus TCP protocol.
The Ethernet server communication module must be connected to an SR3xBXxBDmodular
smart relay with 24VDC supply. Find attached datasheet and instruction manual of SR3NET01BD.
Was this helpful?
What can we do to improve the information ?