Technical FAQs

Ask a Question

Is ION Meters Compatible with IEC 61850 Protocol.

An implementation of IEC 61850 protocol exclusive to the ION7550/7650 platform.
Was this helpful?
What can we do to improve the information ?