Technical FAQs

Ask a Question

How to set the Network Address via DIP Switches in BCPM.

Each BCPM monitor on the daisy chain must have a unique network address from 1–247. Devices with the same address will be
unable to communicate. Set the address before you connect a device to the daisy chain.
 
The values of each DIP switch are listed in below Table.



To determine the address of the monitor, add the values of the switches that are set to ON.
For example, in Figure 7 switch number 4 has an ON value of 8 and switch number 6 has an ON value of 32, so the address is 40 (8 + 32 = 40).



Was this helpful?
What can we do to improve the information ?