Technical FAQs

Ask a Question

Is it allowed to add some wire to extend the lead of a BCPM split core CT.

The standard cable length is 1.8 meter; you may extend the CT leads to
6.1m (20ft), the recommended maximum length for CT extension leads.
Was this helpful?
What can we do to improve the information ?