Technical FAQs

Ask a Question

What register identifies the model number of the BCPM.

The Register 5 identifies the model number of the BCPM.
The values in Register 5 relates to BCPM Model as below;
 
15170 = Model C, current only on all channels, no voltage
15171 = Model B, current only on branch channels, power on channels plus voltage
15172 = Model A, current and power on all channels plus
Was this helpful?
What can we do to improve the information ?