Technical FAQs

Ask a Question

Is it possible to update the firmware of the Altistart 48 control board (VX4G481).

The best way is to order and replace the new control board with the latest version.
It is not possible to update the firmware of Altistart 48 because the µP of the Altistart 48 could not be
flashed. So, an Altistart 48 control board could not be update.
Was this helpful?
What can we do to improve the information ?