Technical FAQs

Ask a Question

What is the procedure for reset APH (Consumption) parameter in Altivar 71 drive.

Here is the procedure for reset APH parameters. It is only possible with the Graphic display terminal.
  1. - Enter in the menu Identification 1.11
  2. - Push enter 2s on the software version of Graphic S.
  3. - Enter in the menu Diagnostic 1.10
  4. - Go to "Test procedure" then push enter
  5. - Go to "RUN Elapsed Time Reset" then push enter
  6. - Go to "Operating t.reset" then push enter
  7. - Choose in the list box "Reset kWh" to reset APH.
Was this helpful?
What can we do to improve the information ?