Technical FAQs

Ask a Question

What is the Inrush Current specification of the Output Contacts of the Tesys T relay.

In the Tesys T, the maximum current of the outputs is 5A up in 250VAC or 30VDC.
Was this helpful?
What can we do to improve the information ?