Technical FAQs

Ask a Question

What is the short circuit current rating (KA) for GV2G** series Comb Busbars.

The short-circuit current withstand rating (KA) of Tesys Comb Busbar is compatible with the breaking capacity of Motor Protection
Circuit Breakers (MPCB) of GV series. The GV Series Comb Busbar does not have a conditional short-circuit current rating.
 
The maximum permissible peak current for GV2G*** Series Comb Busbar is 11KA and for GV3G*64 series Comb Busbar is 20KA.
 
Find attached the Technical datasheet for GV Series Busbars.
 
Was this helpful?
What can we do to improve the information ?