Technical FAQs

Ask a Question

What is the power consumption of ACti9 iC60 overvoltage release units.

The power consumption of ACti9 iC60 overvoltage release units iMSU is 0.002 A at Un ( rated voltage ).
 
Holding : 0.046 VA
 
Inrush : 128 VA
Was this helpful?
What can we do to improve the information ?