Technical FAQs

Ask a Question

What is the difference between the undervoltage coils MN , MNs and MNx of NG125 MCB.

The difference betweenthe undervoltage coils MN , MNx and MNs of NG125 MCB is given below
- undervoltage release
- tripping and opening of the associated circuit-breaker: if supply voltage drops between 70 and 35 %
- reclosing: forbidden if supply voltage is not restored (e.g.: emergency breaking by pushbutton)
- delayed undervoltage release
- allows a 0,25 second time delay on brownout or voltage drop
- undervoltage release unaffected by power cuts.
Was this helpful?
What can we do to improve the information ?