Technical FAQs

Ask a Question

What is the Dielectric Withstand for the Industrial plugs and sockets PK.

Depending upon the rated operating voltage , the test voltage is given below
- up to and including 50V                       test voltage is : 500V
- over 50 up to and including 415V          test voltage is : 2000V
- over 415 up to and including 500V        test voltage is : 2500V
- over 500V                                          test voltage is : 3000V
in according to IEC 60309-1 and IEC60309-2
Was this helpful?
What can we do to improve the information ?