Technical FAQs

Ask a Question

What are the protective function alarms available in Micrologic 5.0/6.0 P trip units.


Below is the list of protective function alarms available in Micrologic 5.0/6.0 P trip units.
 
  • Long-time pickup
  • Short-time pickup
  • Instantaneous pickup
  • Ground-fault current
  • Ground-fault alarm
  • Current unbalance
  • Phase A maximum demand current
  • Phase B maximum demand current
  • Phase C maximum demand current
  • Neutral maximum demand current
  • Minimum voltage (under voltage)
  • Maximum voltage (overvoltage)
  • Voltage unbalance
  • Reverse power
  • Minimum frequency (under frequency)
  • Maximum frequency (over frequency)
  • Phase rotation
  • Current load shedding
  • Power load shedding
Was this helpful?
What can we do to improve the information ?