Technical FAQs

Ask a Question

Can the Masterpact NW shunt trip and shunt close coils be remotely operated.

MX1-COM can be operated remotely by the circuit breaker communication module (BCM).
 
XF-COM can be operated remotely by the electrical close button (BPFE) or remotely by the circuit breaker
 communication module (BCM).
 
Select communicating coil MX/XF as per the supply voltage:-

Communicating Coil (1 part)
AC 50/60 Hz
DC
12 Volts DC
33032
24/30 Volts DC, 24 Volts AC
33033
48/60 Volts DC, 48 Volts AC
33034
100/130 Volts AC/DC
33035
200/250 Volts AC/DC
33036
277 Volts AC
33037
380/480 Volts AC
33038
Was this helpful?
What can we do to improve the information ?