Technical FAQs

Ask a Question

What is the function and ordering part number for the Cradle Communication Module (CCM).

Part reference of Cradle Communication Module (CCM) is 33110.
 
Function of CCM: - The CCM is independent from the Chassis so when the ACB inside the chassis is racked-out the CCM is
still powered and still available on the communication network (Modbus network).
 
For draw-out circuit breakers, the chassis Com manager provides information on the position of the circuit breaker:
> "connected" position
> "test" position
> "disconnected" position.
Was this helpful?
What can we do to improve the information ?