Technical FAQs

Ask a Question

What are the Special features of Micrologic Modbus Addresses.

Special features of Micrologic Modbus addresses;
One circuit breaker uses 3 (fixed versions) or 4 (draw out versions) addresses
@ XX = device module (1 to 47) (the address set on the control unit)
@ XX+50 = chassis module (51 to 97)
@ XX+100 = protection module (101 to 147)
@ XX+200 = measurement module (201 to 247)
 
Example: - If the address 20 is set on the Micrologic control unit, the following addresses are automatically set:
@ 20 (Device Module)
@ 70 (Chassis Module)
@ 120(Protection Module)
@ 220(Measurement Module)
Was this helpful?
What can we do to improve the information ?