Technical FAQs

Ask a Question

How to read breaker status in Circuit Breaker manager test using Modscan software.

Read breaker status using Modscan software
1) Select the address of the concerned manager which is set in Micrologic control unit.
2) Put the register 661
3) Read the information in Binary
Please refer attched example screenshot for more details;
Was this helpful?
What can we do to improve the information ?