Technical FAQs

Ask a Question

How to read Long time protection (Ir) pick-up value in Protection Manager using Modscan software.

Refer the below steps,
 
  1. Select the address of the concerned manager (In our case address 20 is set on the Micrologic control unit hence, Protection Manager @ 20 + 100= 120 
  2. Put the register 875  
  3. Read the "Ir" setting in Amps in Decimal                             
Refer the attached example screenshot to read “Ir” pickup value;
Was this helpful?
What can we do to improve the information ?