Technical FAQs

Ask a Question

How to read rms phase to phase & phase to neutral voltages in Metering Manager using Modscan software.

1) Select the address of the concerned manager (In our case address 20 is set on the Micrologic control unit hence, Metering Manager @ 20 + 200= 220)
2) Put the register 1000
3) Read the value of the voltage V12, V23, V31, V1N, V2N, V3N   volts in Decimal.
Refer the attached example screenshot to read rms voltages using Modscan ;

Was this helpful?
What can we do to improve the information ?