Technical FAQs

Ask a Question

How to send breaker closing commands in shared mode using Modscan software.

 
Step 1: Fill in parameters
 
Register
Datum to be written
7700
57400   (command number)
7701
P1 = 4   (total number of parameters including P1)
7702
P2 = 4   (circuit-breaker manager)
7703
P3 = 0 for Open or P3 = 1 for Close
7704
P4 = 0000 (Password default value)
 
Step 2: Write command
WRITE the previous registers by using function 16 of Modbus protocol.
 
Refer the attached example screenshot to send breaker close/open command using Modscan ;
 
Was this helpful?
What can we do to improve the information ?