Technical FAQs

Ask a Question

What is the difference between a 9001KR4B and 9001KR24B?

Issue:
What is the difference between a 9001KR4B and 9001KR24B?

Product Line:
Harmony Push Buttons

Environment:
Harmony 30mm

Cause:
Product Features

Resolution:
The 9001KR4B has  a snap on plastic mushroom knob and the 9001KR24B has  a screw on plastic mushroom knob with set screw.


CTA-ID : 2060572
Was this helpful?
What can we do to improve the information ?