Technical FAQs

Ask a Question

Is it possible that MV cables be connected other than via the bottom in SM6 cubicle.

All tests were performed with the cables entering from the bottom.
A right or left sided connection would invalidate the test results (internal arcing fault test for connection compartment) because
of the additional holes in the side panels of the cables feed throughs.
 A solution for cable entry via the top is available but not tested (internal fault tests).
Was this helpful?
What can we do to improve the information ?