Technical FAQs

Ask a Question

Which type circuit breaker is used in SM6-36 circuit breaker units.

SF1 type circuit breaker is used in SM6-36 units with circuit breaker.
Was this helpful?
What can we do to improve the information ?