Technical FAQs

Ask a Question

What is the mass and the volume bottle of SF6 gas in the SM6-36 cubicles.

Mass of the switch filled with SF6 gas under 1.5bar relative : 68kG
Mass of the SF6 gas under 1.5bar pressure: 0.8kG
Volume of the switch (bottle): 77dm3
Was this helpful?
What can we do to improve the information ?