Technical FAQs

Ask a Question

Which side of the SM6-36 cubicle internal arc protection is available.

Internal arc protection is provided in front of the cubicles, there are special flaps rear sides of the cubicle to
 release gas pressure through the right direction.
Was this helpful?
What can we do to improve the information ?