Technical FAQs

Ask a Question

How do the LF circuit breakers behave at 0 bars SF6 pressure.

At 0 bar SF6, LF range circuit breakers are capable of breaking their rated current at their rated voltage.
 
It retains 80% of their dielectric withstand and will be able to break 80% of their short circuit current.
Was this helpful?
What can we do to improve the information ?