Technical FAQs

Ask a Question

What is the difference between the cubicles type PM & QM in SM6 cubicle.

QM- fuse switch combination unit
 
PM- fuse switch unit
 
It means with QM type cubicle, the system is tripped if the one fuse is melt, but with the PM type the system will work on 2 fuses.
 
Was this helpful?
What can we do to improve the information ?