Technical FAQs

Ask a Question

Is it possible to install Easypact CVS MCCBs side by side horizontally or vertically with zero distance between the two consecutive MCCBs.

The Easypact CVS MCCBs can be installed both horizontally and vertically with the zero distance between the two consecutive
MCCBs but at the same time, the rules given in the standard catalogue (attached below) must be followed. It is recommended
to use interphase barriers or terminal shield to ensure insulation of live parts, unless insulated bars are used to connect devices
and busbar.
Was this helpful?
What can we do to improve the information ?