Technical FAQs

Ask a Question

Where is the thickness of rear insulating screen of Compact NSX MCCB.

The thickness of rear insulating screen of Compact NSX 100/160/250 and Compact NSX 400/630 are 1 mm and 1.5 mm respectively.
 
Please refer the below snapshot for details.
The Compact NSX DC-PV is a non-polarized MCCB.
 
Was this helpful?
What can we do to improve the information ?