Technical FAQs

Ask a Question

How many channels are included in one Acti 9 Smartlink module.

Acti 9 Smartlink is equipped with 11 (Eleven) 24 V DC channels. Each channel is represented by a Ti24.
Ti24 interface consisting of:
  1. Two power supply terminals: 0 V and 24 V DC
  2. Two 24 V DC logic inputs (I1 and I2),
  3. One 24 V DC logic output (Q)
Was this helpful?
What can we do to improve the information ?