Technical FAQs

Ask a Question

What is the Acti9 communication block diagram.

The Acti 9 communication system is simple and safe to use:
 All Acti 9 communication system functions can be created by sending messages (Modbus protocol) to Acti 9
Smartlink devices (Modbus slaves) that act on devices via Ti24 interfaces.
 
Acti 9 Communication System Block Diagram is illustrated in attachment;
Was this helpful?
What can we do to improve the information ?