Technical FAQs

Ask a Question

The table below describes the various devices in the Acti 9 range that can be connected to the Acti 9 Smartlink device.


The table below describes the various devices in the Acti 9 range that can be connected to the Acti 9 Smartlink device:
 
Designation
Reference
Description
iACT24
A9C15924
Contactor control switch
iATL24
A9C15424
Impulse relay control switch
iOF+SD24
A9A26897
Indication auxiliary with Ti24 interface for iC60 circuit breaker
OF+SD24
A9N26899
Indication auxiliary with Ti24 interface for C60, C120 circuit
breaker
RCA iC60 with Ti24
Interface
A9C7012•
Remote control with Ti24 interface
Reflex iC60 with Ti24 interface
A9C6••••
Integrated control circuit breaker with Ti24 interface
 
Was this helpful?
What can we do to improve the information ?