Technical FAQs

Ask a Question

How to reset to the Acti 9 Smartlink device to factory default values.

To reset the Acti 9 Smartlink device, proceed as follows:
De-energize Acti 9 Smartlink
Set the Modbus address to value 00
Re-energize Acti 9 Smartlink
The reset data is as follows:
  1. The communication parameters become: 19,200 baud, even parity, 1 stop bit
  2. The operation counters are set to 0
  3. The running hours counters are set to 0
  4. The counter modification dates are set to the value "1 January 2000"
  5. The counter pulse weights are set to 10
Was this helpful?
What can we do to improve the information ?