Technical FAQs

Ask a Question

What are the ways to communicate between the PC and the Acti 9 Smartlink devices.

Communication between the PC and the Acti 9 Smartlink devices can be done by 2 ways:
 
Ethernet TCP-IP wiring: through an EGX••• gateway with a Ethernet cable with 2 RJ45 connectors
 
Modbus Serial Line wiring: through a specific link with a USB-Modbus Serial Line cable (A9XCATM1 reference)
 
Was this helpful?
What can we do to improve the information ?