Technical FAQs

Ask a Question

What is the max duty cycle for the ATS01 soft starters?



ATS01N1...FT
1 second start time, 100 maximum number of starts per hour
5 second start time, 20 maximum number of starts per hour

ATS01N2206 to N222, LU, QN, RT
1 second start time, 100 maximum number of starts per hour
5 second start time, 20 maximum number of starts per hour
10 second start time, 10 maximum number of starts per hour

ATS01N232, LU, QN, RT
1 second start time, 50 maximum number of starts per hour
5 second start time, 10 maximum number of starts per hour
10 second start time, 5 maximum number of starts per hour

ATS01N2... LY, Q
1 second start time, 360 maximum number of starts per hour
12 second start time, 30 maximum number of starts per hour
 

Was this helpful?
What can we do to improve the information ?