Technical FAQs

Ask a Question

How to update the firmware of the TCSESM Ethernet Managed Switches.

Follow the procedure to update the firmware of the Ethernet managed switch. 

1. Open the webpage by typing the IP address of the Switch.
2. Go to Software and use Http software update to update the firmware of the TCSESM Ethernet switch. 
3. Once loaded successfully it should show the message “Update successfully“. 
4. Now go to Restart >> Cold start. 

Was this helpful?
What can we do to improve the information ?