Technical FAQs

Ask a Question

What does error code E733F mean on a Lexium 32 drive.

Error code E733F means the amplitude of the Encoder analog signals is too low. This could mean that the
problem may be usually with the Encoder or the encoder feedback cable. It makes sense to verify if the user
is using non-Schneider custom made feedback cables. A high interference to the feedback cable/system is
another possibility.
Some of the other points that could be checked are the ambient temperature and current
Motor temperature. (Parameter _M_T_Current - Modbus parameter # 7202).
 
An EMC check on the site can help if the above does not resolve.
Was this helpful?
What can we do to improve the information ?