Technical FAQs

Ask a Question

What is the derating for high altitude application for Altivar 32.

Up to 1000 meter without derating, 1000 to 3000 meter derating the current by 1 % per additional 100 meter.
Was this helpful?
What can we do to improve the information ?