Technical FAQs

Ask a Question

What is the difference between a TVSS type EMA and EBA device ?

The EMA series TVSS devices have one module per phase where the EBA TVSS devices have one module (brick) that connects to all phases.  The EBA series TVSS also has a top surge current rating of 240kAper phase.  The EMA series TVSS devices include the larger surge current ratings of 320kA per phase and 480kA per phase.


CTA-ID : 2061146
Was this helpful?
What can we do to improve the information ?