Technical FAQs

Ask a Question

How to remove the error “Cannot write to C:/Projects\Vijeo Citect v7.20\User\Projrct_Test\_supergenie.ctm” while saving the super genie in VJC 7.20

You may remove this error by deleting the file "_supergenie.TMP" which is a temporary file created having the same size as "_supergenie.ctm " in
 the Citect . Delete that file and after that restarted Citect Explore.  Also recommendations for this error are first uncheck "Fast Update Pages" from
Graphic builder >> tools >> options.
Always after modification in supergenies or genies use pack libraries and update pages in graphic builder >> tools .
Was this helpful?
What can we do to improve the information ?