Technical FAQs

Ask a Question

What is the trend file size limits that we can store in Vijeo Citect V 7.20 .

There is no such limitation for the trend file size , any amount of data can be collected and stored. The only restriction on the
 amount of data that you can store is the size of the hard disk on your computer (an efficient data storage method is used to
optimize the use of storage space on your computer's hard disk). For long term storage, you can archive the data to disk or
tape (without disrupting your runtime system).
Was this helpful?
What can we do to improve the information ?