Technical FAQs

Ask a Question

How can we configure a popup so that it should always remain in front , till operator does not close it.

User can use WinNewAt( "page name", X, Y , 65) to open a popup which will always remains in front of page.
 
Where :
Page name: The name or page number of the page to display (in quotation marks ""). Can be prefixed by the name of a host
cluster, that is "ClusterName.Page". This will take precedence over the use of the ClusterName parameter if the two differ.
 
X: The x pixel coordinate of the top left corner of the window.
 
Y: The y pixel coordinate of the top left corner of the window.
 
65: Mode(Always on top + Page child window)
Was this helpful?
What can we do to improve the information ?