Technical FAQs

Ask a Question

I am facing a problem in establishing the server-client setup between a VJC 7.20 SCADA system with Full license and a system with Control client license.

User need to check the following points,
1-Both the Server and Client system should have the same SCADA version and Service Pack, if they have different version
or service pack then change the INI parameter [LAN]EarliestLegacyVersion accordingly.

2-Check that in both Server and Client system should have same “Default Server Password” in Computer Setup Wizard.
Was this helpful?
What can we do to improve the information ?