Technical FAQs

Ask a Question

What is the power dissipation of Tesys LT3 thermal protection units.

The average consumption/dissipation values are 2.5VA for AC supply and 1W for DC supply is valid for entire
 temperature operating range with accuracy of +-15%.
 
Please refer the attachment for the details.
Was this helpful?
What can we do to improve the information ?