Technical FAQs

Ask a Question

Is it possible to make the datalogging on a M258 directly to a USB Stick instead to the filesystem and access via FTP Server.

The Data Logging function always will store the files to the PLC file system, and there is no possibility to select a different storage location.
You can transfer the Data Logging files either by event or periodically from the PLC file system to the USB stick.
With "PLC_R.i_wUSBHostStatus", it should be possible to detect event from application.
Was this helpful?
What can we do to improve the information ?