Technical FAQs

Ask a Question

How many connection can have at the same time with one HMISTU to the PLCs over Modbus RTU or Ethernet TCP/IP Modbus.

The HMISTU can support up to 48 Modbus TCP/IP devices.
The recommended number for Modbus RTU is 32 devices.
Was this helpful?
What can we do to improve the information ?