Technical FAQs

Ask a Question

How do you wire up a 24vdc push pull encoder to the VW3A3407 encoder option card for the ATV71 drive?

The pin outs may vary depending on the encoder type and connector type.

Basic setup is as follows:
A from the encoder goes to A on the encoder card
B from the encoder goes to B on the encoder card
A not and B not are tied together and jumper to 0V on the encoder card.
+24vdc goes to +V encoder card
0V goes to 0V on the encoder card


Was this helpful?
What can we do to improve the information ?