Technical FAQs

Ask a Question

In which memory location the values are stored for Function block internal parameters M001 to M008 for Altivar 32 drive.

For Altivar 32, there are total 8 numbers of internal function block parameters M001 to M008. Values written to M001 to M004
are stored in flash memory whereas values on M005 to M008 are stored with RAM. So, Values stored on M001 to M004 remains
retained even after power cycle of drive. Values on M005 to M008 get reset with power cycle.
Was this helpful?
What can we do to improve the information ?