Technical FAQs

Ask a Question

How long application can remain in M218 logic controller without power.

In M218, application is written to a flash memory and so application remains forever without need of battery or external power supply.
Was this helpful?
What can we do to improve the information ?